LPC55S69 Firmware Update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 Firmware Update

2,699 Views
zhangeh10594
Contributor III

Hello,I'm not find the LPC55S69 firmware update examples,but I find this :

pastedImage_1.png

and one of its code was pastedImage_2.png

so ,what the code means? It is an example for LPC54608 not for LPC55S69? I wonder if the examples also suit for LPC55S69. And if not,how the LPC55S69 firmware update go?

    Please!

Labels (1)
3 Replies

2,561 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 小白 张

AN12327sw is for LPC55s69, not for LPC54608.

Which file/line in AN12327sw included this trace code? Please let me know, I will check.



Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,561 Views
zhangeh10594
Contributor III

Hi ZhangJennie

 Sorry too late to reply. The code is line in 200 line ,in the project of dsbl.eww. and the project trace is ......AN12327SW\boards\lpcxpresso55s69\dual_sbl\lpc55xx_dsbl\cm33_core0\iar.

So if this code isn't correct , could you please give me a link to the correct one.Thanks.

0 Kudos
Reply

2,561 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

this is a typo issue. The function should be correct. please change the trace message from lpc54608 to lpc55S69.

if any function issue, please let me know.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------