LPC55S69 Execute ISP Command

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 Execute ISP Command

1,581 次查看
awseiger
Contributor I

Hello,

When I send the "execute" command to the ISP ROM bootloader, the LPC55S69 responds with "Command is Not Supported (0x2716). The user manual claims that this is a supported command, and "get-property available-commands" shows that execute is a valid command. What am I doing wrong? I am trying to execute a program that I have loaded into RAM via an SB2.1 upload.

Thanks,

Alex

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,574 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Alex,

Do you use blhost ?

Could you please show all your steps and all the commands?

If you want to use secure boot, recommend you refer to this application note:

https://www.nxp.com.cn/docs/en/application-note/AN12283.pdf 

 

Regards,

Alice

0 项奖励
回复