LPC55S69 Execute ISP Command

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 Execute ISP Command

1,576件の閲覧回数
awseiger
Contributor I

Hello,

When I send the "execute" command to the ISP ROM bootloader, the LPC55S69 responds with "Command is Not Supported (0x2716). The user manual claims that this is a supported command, and "get-property available-commands" shows that execute is a valid command. What am I doing wrong? I am trying to execute a program that I have loaded into RAM via an SB2.1 upload.

Thanks,

Alex

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,569件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Alex,

Do you use blhost ?

Could you please show all your steps and all the commands?

If you want to use secure boot, recommend you refer to this application note:

https://www.nxp.com.cn/docs/en/application-note/AN12283.pdf 

 

Regards,

Alice

0 件の賞賛
返信