LPC55S69-EVK board not recognized by PC through USB debug probe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69-EVK board not recognized by PC through USB debug probe

1,760件の閲覧回数
manuardi
Contributor II

Very Basic question : At first connection the board LPC55S69-EVK is not recognized when connecting it to the PC through "Debug probe" USB connector  : Windows tells the driver for the board is not found. I could not find indication in documentation that such driver should be uploaded ? It looks strange since no one on the forum seems to have had this issue. Note that on this same USB port of the PC , I have some times ago connected other type of NXP EVK board and it worked properly without having any specific driver to load. NB : of course I have loaded the board SDK beforehand.

0 件の賞賛
返信
2 返答(返信)

1,679件の閲覧回数
manuardi
Contributor II

Well, I reply to this one myself ! you HAVE TO load and install MCUXpressoIDE even if you use other IDEs (IAR in my case). This is not intuitive and should be indicated somewhere in the getting started page. Best regards.

0 件の賞賛
返信

1,679件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Manu ARDI,

OK, thanks for your sharing.

BR

Alice

0 件の賞賛
返信