LPC55S69 EVK Board - SPI Testing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55S69 EVK Board - SPI Testing

跳至解决方案
2,603 次查看
SrinathVelavan
Contributor III

I am trying to test out the SPI interface on the LPC55S69 EVK board. Tried the spi_polling_b2b_transfer_master code from the SDK and the Master Start was successfully obtained with loop-back mechanism. 

Now, am looking to get the same output without the help of loopback mechanism. Any help on this will be much appreciated. 

Also, Is the LPC55S69 and LPC4322FET100E connected together on the EVK? If so, what is the use of the LPC4322 on the EVK board?

#spi #lpc55s69

0 项奖励
回复
1 解答
2,592 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

EVK board equipted On-board (Link2) Debug probe, LPC4322 is the MCU for the debug probe.

On board LPC4322 is neither SPI master nor slave. 

LPC55 SPI communication.

The spi_polling_board2board_master example shows how to use spi driver as master to do board to board transfer with polling.

n this example, one spi instance as master and another spi instance on othereboard as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.

In order to run this demo, two LPCXpresso55s69 boards are needed.

Thanks,

Jun Zhang

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,593 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

EVK board equipted On-board (Link2) Debug probe, LPC4322 is the MCU for the debug probe.

On board LPC4322 is neither SPI master nor slave. 

LPC55 SPI communication.

The spi_polling_board2board_master example shows how to use spi driver as master to do board to board transfer with polling.

n this example, one spi instance as master and another spi instance on othereboard as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.

In order to run this demo, two LPCXpresso55s69 boards are needed.

Thanks,

Jun Zhang

0 项奖励
回复
2,589 次查看
SrinathVelavan
Contributor III

In the second board, How do I configure it to be the slave in the polling code example?

0 项奖励
回复
2,590 次查看
SrinathVelavan
Contributor III
Thank you very much for the clarification. I ll try the same with the 2 EVKs.
0 项奖励
回复