LPC55S69 EVK Board - SPI Testing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 EVK Board - SPI Testing

Jump to solution
2,622 Views
SrinathVelavan
Contributor III

I am trying to test out the SPI interface on the LPC55S69 EVK board. Tried the spi_polling_b2b_transfer_master code from the SDK and the Master Start was successfully obtained with loop-back mechanism. 

Now, am looking to get the same output without the help of loopback mechanism. Any help on this will be much appreciated. 

Also, Is the LPC55S69 and LPC4322FET100E connected together on the EVK? If so, what is the use of the LPC4322 on the EVK board?

#spi #lpc55s69

0 Kudos
Reply
1 Solution
2,611 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

EVK board equipted On-board (Link2) Debug probe, LPC4322 is the MCU for the debug probe.

On board LPC4322 is neither SPI master nor slave. 

LPC55 SPI communication.

The spi_polling_board2board_master example shows how to use spi driver as master to do board to board transfer with polling.

n this example, one spi instance as master and another spi instance on othereboard as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.

In order to run this demo, two LPCXpresso55s69 boards are needed.

Thanks,

Jun Zhang

View solution in original post

0 Kudos
Reply
3 Replies
2,612 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

EVK board equipted On-board (Link2) Debug probe, LPC4322 is the MCU for the debug probe.

On board LPC4322 is neither SPI master nor slave. 

LPC55 SPI communication.

The spi_polling_board2board_master example shows how to use spi driver as master to do board to board transfer with polling.

n this example, one spi instance as master and another spi instance on othereboard as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct.

In order to run this demo, two LPCXpresso55s69 boards are needed.

Thanks,

Jun Zhang

0 Kudos
Reply
2,608 Views
SrinathVelavan
Contributor III

In the second board, How do I configure it to be the slave in the polling code example?

0 Kudos
Reply
2,609 Views
SrinathVelavan
Contributor III
Thank you very much for the clarification. I ll try the same with the 2 EVKs.
0 Kudos
Reply