LPC55S69: Cannot write CFPA after sealing CMPA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69: Cannot write CFPA after sealing CMPA

ソリューションへジャンプ
1,793件の閲覧回数
HenrikK
Contributor II

After writing CMPA with Secureboot enabled and sealed, I cannot write CFPA anymore.

 

$ blhost -p /dev/ttyPS1 -- write-memory 0x0009DE00 cfpa.bin 
Ping responded in 1 attempt(s)
Inject command 'write-memory'
Preparing to send 512 (0x200) bytes to the target.
Response status = 10001 (0x2711) Command disallowed when security is enabled.
Wrote 0 of 512 bytes.

$ blhost -p /dev/ttyPS1 -- get-property 17
Ping responded in 1 attempt(s)
Inject command 'get-property'
Response status = 0 (0x0) Success.
Response word 1 = 3275539260 (0xc33cc33c)
Security State = SECURE

 

This is really puzzling because I read AN12283 and UM11126 and nothing indicates that sealing CMPA would seal CFPA too. This behavior also does not make sense to me because it would prevent any software updates. I'm not sure about the content of my cfpa.bin but I would expect a more detailed error code like "kStatus_FLASH_CfpaScratchPageInvalid" in that case.

Is this intended or am I missing some detail?

タグ(3)
0 件の賞賛
返信
1 解決策
1,752件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @HenrikK 

I'm sorry for the  puzzling for you.

I will take a ticket to request add some description about "seal" function.

"Is this intended or am I missing some detail?"

->> And sorry yes, it is intended. 

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,753件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @HenrikK 

I'm sorry for the  puzzling for you.

I will take a ticket to request add some description about "seal" function.

"Is this intended or am I missing some detail?"

->> And sorry yes, it is intended. 

 

BR

Alice

0 件の賞賛
返信