LPC55S69: Cannot write CFPA after sealing CMPA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69: Cannot write CFPA after sealing CMPA

Jump to solution
1,789 Views
HenrikK
Contributor II

After writing CMPA with Secureboot enabled and sealed, I cannot write CFPA anymore.

 

$ blhost -p /dev/ttyPS1 -- write-memory 0x0009DE00 cfpa.bin 
Ping responded in 1 attempt(s)
Inject command 'write-memory'
Preparing to send 512 (0x200) bytes to the target.
Response status = 10001 (0x2711) Command disallowed when security is enabled.
Wrote 0 of 512 bytes.

$ blhost -p /dev/ttyPS1 -- get-property 17
Ping responded in 1 attempt(s)
Inject command 'get-property'
Response status = 0 (0x0) Success.
Response word 1 = 3275539260 (0xc33cc33c)
Security State = SECURE

 

This is really puzzling because I read AN12283 and UM11126 and nothing indicates that sealing CMPA would seal CFPA too. This behavior also does not make sense to me because it would prevent any software updates. I'm not sure about the content of my cfpa.bin but I would expect a more detailed error code like "kStatus_FLASH_CfpaScratchPageInvalid" in that case.

Is this intended or am I missing some detail?

0 Kudos
Reply
1 Solution
1,748 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @HenrikK 

I'm sorry for the  puzzling for you.

I will take a ticket to request add some description about "seal" function.

"Is this intended or am I missing some detail?"

->> And sorry yes, it is intended. 

 

BR

Alice

View solution in original post

0 Kudos
Reply
1 Reply
1,749 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @HenrikK 

I'm sorry for the  puzzling for you.

I will take a ticket to request add some description about "seal" function.

"Is this intended or am I missing some detail?"

->> And sorry yes, it is intended. 

 

BR

Alice

0 Kudos
Reply