LPC55S69 : CASPER and Core1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 : CASPER and Core1

1,284 次查看
EugeneHiihtaja
Senior Contributor I

Hello !

In UM mentioned:

"

ARMv8-M architecture (ARM M33) introduces co-processor interface allowing CASPER
access via MCR (Move from Coprocessor to Register) and MRC (Move from Register to
Coprocessor) opcodes. Using this, up to two registers can be transferred between ARM
M33 core and CASPER.

"

If Casper act as coprocessor and Core1 dosn't supports coprocessors, it means CASPER can't be used from Core1 ?

Is this so ?

MPU, FPU, DSP, ETM, Trustzone (SECEXT), Secure Attribution Unit (SAU) or co-processor interface are not avaible on Core1.

What other peripherals can't be used from Core1 ?

What areas of SRAM are recommended for code execution for Core1 ?

Regards,

Eugene

0 项奖励
回复
1 回复

1,223 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Eugene

What do you mean " it means CASPER can't be used from Core1 "?

Casper is a accelerator engine. it's not a coprocessor.
Casper Sits on Cortex-M33 co-processor bus. An AHB bus and ARMv8-M Coprocessor (CP) interface to allow loading information to perform operations.
It works standalone from co-processor. Using CASPER can free up the ARM M33 to do other tasks while CASPER does the computation.

Fast shared RAM access 2x 32b RAMs which are allocated for CASPER RAM interface and shared with System Memory.

For Casper engine, I recommend a useful document:

https://www.nxp.com/docs/en/application-note/AN12445.pdf 

https://www.nxp.com/docs/en/application-note-software/AN12445SW.zip 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复