LPC55S36, I3C GETMRL issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S36, I3C GETMRL issue

Jump to solution
5,923 Views
bell_huang
Contributor III

I'm running I3C on LPC5536-EVK and find out that GETMRL command doesn't seem to work for any of the sensors. This issue can be reproduced in Building an I3C Sensor Network Using LPC553x/LPC55S3x example.

 

To begin with the conclusion: if GETMRL reads 3 bytes, it gets stuck after reading two bytes. However, if GETMRL reads only 2 bytes, it does not get stuck.

 

SDK: SDK_2.16.000_LPCXpresso55S36 

 

At the beginning, if we call the I3C_BusMasterGetDeviceInfo() function from fsl_component_i3c.h, the function will get stuck. The I3C_BusMasterGetDeviceInfo() function includes several commands, such as GETPID, GETBCR, GETDCR, GETMRL, and GETMWL.

To simplify things, we copied out the two functions I3C_BusMasterGetBCR (GETBCR) and I3C_BusMasterGetMaxReadLength (GETMRL) and tested them individually.

static status_t I3C_BusMasterGetBCR(i3c_device_t *master, i3c_device_information_t *info)
{
    uint8_t bcr;
    i3c_ccc_cmd_t getBCRCmd = {0};
    status_t result         = kStatus_Success;

    getBCRCmd.isRead   = true;
    getBCRCmd.cmdId    = I3C_BUS_CCC_GETBCR;
    getBCRCmd.destAddr = info->dynamicAddr;
    getBCRCmd.data     = &bcr;
    getBCRCmd.dataSize = 1U;

    result = I3C_BusMasterSendCCC(master, &getBCRCmd);

    info->bcr = bcr;

    return result;
}

static status_t I3C_BusMasterGetMaxReadLength(i3c_device_t *master, i3c_device_information_t *info)
{
    i3c_ccc_cmd_t getMRLCmd = {0};
    status_t result         = kStatus_Success;

    getMRLCmd.isRead   = true;
    getMRLCmd.cmdId    = I3C_BUS_CCC_GETMRL;
    getMRLCmd.destAddr = info->dynamicAddr;
    getMRLCmd.data     = malloc(3U);
    getMRLCmd.dataSize = 3U;

    /*
     * When the device does not have IBI payload GETMRL only returns 2
     * bytes of data.
     */
    if ((info->bcr & I3C_BUS_DEV_BCR_IBI_PAYLOAD_MASK) == 0U)
    {
        getMRLCmd.dataSize -= 1U;
    }

    result = I3C_BusMasterSendCCC(master, &getMRLCmd);

    uint8_t *pData = getMRLCmd.data;
    if ((info->bcr & I3C_BUS_DEV_BCR_IBI_PAYLOAD_MASK) != 0U)
    {
        info->maxIBILength = pData[2];
    }

    info->maxReadLength = (uint16_t)pData[0] << 8UL | (uint16_t)pData[1];

    free(getMRLCmd.data);

    return result;
}

 

Then we can reproduce the stuck issue by calling them:

i3c_device_information_t device_info;
memset(&device_info, 0, sizeof(device_info));
device_info.dynamicAddr = icm42688p_sensorAddr;
I3C_BusMasterGetBCR(&demo_masterDev, &device_info);
I3C_BusMasterGetMaxReadLength(&demo_masterDev, &device_info);

After checking the waveform, we found that it gets stuck at GETMRL. After reading the MRL LSB, the SCL line stops and doesn't move anymore.

bell_huang_0-1744790912809.png

 

In previous case, I3C_BusMasterGetBCR reads the BCR value of the ICM42688P as 39 (= b00100111), which indicates that it supports BCR[2] IBI Payload. As a result, The dataSize of GETMRL in I3C_BusMasterGetMaxReadLength is 3.

 

If we assume that it does not support BCR[2] IBI Payload, that is, do not call I3C_BusMasterGetBCR, then the dataSize of GETMRL in I3C_BusMasterGetMaxReadLength is 2.

i3c_device_information_t device_info;
memset(&device_info, 0, sizeof(device_info));
device_info.dynamicAddr = icm42688p_sensorAddr;
//I3C_BusMasterGetBCR(&demo_masterDev, &device_info);
I3C_BusMasterGetMaxReadLength(&demo_masterDev, &device_info);

Then we can see GETMRL workable, it no longer gets stuck.

bell_huang_0-1744791335331.png

 

In MIPI I3C Basic℠ v1.1.1 , 5.1.9.3.6 Set/Get Max Read Length (SETMRL/GETMRL), the 3rd byte is IBI Payload Size which is optional. That is, if the sensor support IBI Payload, GETMRL shall read 3 bytes. But in current SDK, it seems get stuck if we read 3 bytes.

bell_huang_1-1744791750013.png

 

 

 

0 Kudos
Reply
1 Solution
5,677 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @bell_huang

I am using the latest I3C driver file (MAKE_VERSION(2, 13, 1)), and when the data size is 3, it no longer locks up. After confirming with the SDK team, there is indeed an update. So you can test it.
Although there is no lock, the 3rd byte is not received. After analysis, it appears that the slave actively terminated the read operation. So you can try to another sensor or consult the sensor manufacturer for further assistance.

BR

Harry

 

View solution in original post

0 Kudos
Reply
8 Replies
5,892 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @bell_huang 

In order to reproduce this issue quickly.

Can you share the i3c_master_read_sensor_icm42688p.c?

BR

Harry

0 Kudos
Reply
5,810 Views
bell_huang
Contributor III

Hi @Harry_Zhang ,

Can you reproduce with attached i3c_sensor_network.c ?

0 Kudos
Reply
5,678 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @bell_huang

I am using the latest I3C driver file (MAKE_VERSION(2, 13, 1)), and when the data size is 3, it no longer locks up. After confirming with the SDK team, there is indeed an update. So you can test it.
Although there is no lock, the 3rd byte is not received. After analysis, it appears that the slave actively terminated the read operation. So you can try to another sensor or consult the sensor manufacturer for further assistance.

BR

Harry

 

0 Kudos
Reply
5,660 Views
bell_huang
Contributor III

Hi @Harry_Zhang ,

Thanks for your test. Can you share the link of latest I3C driver file (MAKE_VERSION(2, 13, 1))? I cannot find it out in MCUXpresso SDK Dashboard . There are only 25.03.00, 2.16.000, 2.15.000.

 

I test LSM6DST which is an another sensor that supports GETMRL 3 bytes. The original I3C driver doesn't lock.

bell_huang_0-1745820964321.png

 

In comparison, ICM42688P pulls low the T-bit of LSB byte to indicate the end of the data. It means that if the sensor doesn't support GETMRL 3 bytes and the original driver want to read 3 bytes, then it will be locked.

bell_huang_1-1745821562842.png

 

I think the best is: The GETMRL function returns fail/error status if the driver want to read 3 bytes and the sensor doesn't support 3 bytes (pull low the T-bit of LSB byte).

However, it is acceptable: The GETMRL function will not lock at least.

 

 

 

0 Kudos
Reply
5,656 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @bell_huang 

You can download the latest  25.03.00 SDK.

Harry_Zhang_0-1745823160002.png

"I think the best is: The GETMRL function returns fail/error status if the driver want to read 3 bytes and the sensor doesn't support 3 bytes (pull low the T-bit of LSB byte)."

Thank you for your suggestion. I will report it to the SDK team. Hope to improve in the future.

BR

Harry

0 Kudos
Reply
5,576 Views
bell_huang
Contributor III

Thanks. I tested IDE v24.12.148 & SDK 25.03.00. The GETMRL no longer get stuck.

Test step:

(1) Import SDK example(s)... -> driver_examples -> i3c ->i3c_master_read_sensor_icm42688p

(2) Remove source/i3c_master_read_sensor_icm42688p.c

(3) Add attached i3c_sensor_network.c to source/i3c_sensor_network.c

0 Kudos
Reply
5,791 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @bell_huang 

Yes, i can reproduce this issue, I am investigating this issue.

BR

Harry

0 Kudos
Reply
5,861 Views
bell_huang
Contributor III

Hi @Harry_Zhang ,

This issue can be reproduced in Building an I3C Sensor Network Using LPC553x/LPC55S3x example.

 

0 Kudos
Reply
%3CLINGO-SUB%20id%3D%22lingo-sub-2081547%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ELPC55S36%2C%20I3C%20GETMRL%20issue%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2081547%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%3CSPAN%3EI'm%20running%20I3C%20on%26nbsp%3B%3C%2FSPAN%3E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fdesign-center%2Fsoftware%2Fdevelopment-software%2Fmcuxpresso-software-and-tools-%2Flpcxpresso-boards%2Flpcxpresso55s36-development-board%3ALPCXpresso55S36%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3ELPC5536-EVK%3C%2FA%3E%3CSPAN%3E%26nbsp%3Band%20find%20out%20that%20%3CSTRONG%3EGETMRL%3C%2FSTRONG%3E%20command%20doesn't%20seem%20to%20work%20for%20any%20of%20the%20sensors.%26nbsp%3B%3C%2FSPAN%3E%3CSPAN%3EThis%20issue%20can%20be%20reproduced%20in%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note-software%2FAN13577SW.zip%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EBuilding%20an%20I3C%20Sensor%20Network%20Using%20LPC553x%2FLPC55S3x%3C%2FA%3E%26nbsp%3Bexample.%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CP%3ETo%20begin%20with%20the%20conclusion%3A%20if%20%3CSTRONG%3EGETMRL%3C%2FSTRONG%3E%20reads%203%20bytes%2C%20it%20gets%20stuck%20after%20reading%20two%20bytes.%20However%2C%20if%20%3CSTRONG%3EGETMRL%3C%2FSTRONG%3E%20reads%20only%202%20bytes%2C%20it%20does%20not%20get%20stuck.%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%3CSPAN%3ESDK%3A%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fmcuxpresso.nxp.com%2Fen%2Fdashboard%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3ESDK_2.16.000_LPCXpresso55S36%3C%2FA%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CP%3EAt%20the%20beginning%2C%20if%20we%20call%20the%20I3C_BusMasterGetDeviceInfo()%20function%20from%20fsl_component_i3c.h%2C%20the%20function%20will%20get%20stuck.%20The%20I3C_BusMasterGetDeviceInfo()%20function%20includes%20several%20commands%2C%20such%20as%20GETPID%2C%20GETBCR%2C%20GETDCR%2C%20%3CSTRONG%3EGETMRL%3C%2FSTRONG%3E%2C%20and%20GETMWL.%3C%2FP%3E%3CP%3ETo%20simplify%20things%2C%20we%20copied%20out%20the%20two%20functions%20I3C_BusMasterGetBCR%20(GETBCR)%20and%20I3C_BusMasterGetMaxReadLength%20(%3CSTRONG%3EGETMRL%3C%2FSTRONG%3E)%20and%20tested%20them%20individually.%3C%2FP%3E%3CPRE%20class%3D%22lia-code-sample%20language-cpp%22%3E%3CCODE%3Estatic%20status_t%20I3C_BusMasterGetBCR(i3c_device_t%20*master%2C%20i3c_device_information_t%20*info)%0A%7B%0A%20%20%20%20uint8_t%20bcr%3B%0A%20%20%20%20i3c_ccc_cmd_t%20getBCRCmd%20%3D%20%7B0%7D%3B%0A%20%20%20%20status_t%20result%20%20%20%20%20%20%20%20%20%3D%20kStatus_Success%3B%0A%0A%20%20%20%20getBCRCmd.isRead%20%20%20%3D%20true%3B%0A%20%20%20%20getBCRCmd.cmdId%20%20%20%20%3D%20I3C_BUS_CCC_GETBCR%3B%0A%20%20%20%20getBCRCmd.destAddr%20%3D%20info-%26gt%3BdynamicAddr%3B%0A%20%20%20%20getBCRCmd.data%20%20%20%20%20%3D%20%26amp%3Bbcr%3B%0A%20%20%20%20getBCRCmd.dataSize%20%3D%201U%3B%0A%0A%20%20%20%20result%20%3D%20I3C_BusMasterSendCCC(master%2C%20%26amp%3BgetBCRCmd)%3B%0A%0A%20%20%20%20info-%26gt%3Bbcr%20%3D%20bcr%3B%0A%0A%20%20%20%20return%20result%3B%0A%7D%0A%0Astatic%20status_t%20I3C_BusMasterGetMaxReadLength(i3c_device_t%20*master%2C%20i3c_device_information_t%20*info)%0A%7B%0A%20%20%20%20i3c_ccc_cmd_t%20getMRLCmd%20%3D%20%7B0%7D%3B%0A%20%20%20%20status_t%20result%20%20%20%20%20%20%20%20%20%3D%20kStatus_Success%3B%0A%0A%20%20%20%20getMRLCmd.isRead%20%20%20%3D%20true%3B%0A%20%20%20%20getMRLCmd.cmdId%20%20%20%20%3D%20I3C_BUS_CCC_GETMRL%3B%0A%20%20%20%20getMRLCmd.destAddr%20%3D%20info-%26gt%3BdynamicAddr%3B%0A%20%20%20%20getMRLCmd.data%20%20%20%20%20%3D%20malloc(3U)%3B%0A%20%20%20%20getMRLCmd.dataSize%20%3D%203U%3B%0A%0A%20%20%20%20%2F*%0A%20%20%20%20%20*%20When%20the%20device%20does%20not%20have%20IBI%20payload%20GETMRL%20only%20returns%202%0A%20%20%20%20%20*%20bytes%20of%20data.%0A%20%20%20%20%20*%2F%0A%20%20%20%20if%20((info-%26gt%3Bbcr%20%26amp%3B%20I3C_BUS_DEV_BCR_IBI_PAYLOAD_MASK)%20%3D%3D%200U)%0A%20%20%20%20%7B%0A%20%20%20%20%20%20%20%20getMRLCmd.dataSize%20-%3D%201U%3B%0A%20%20%20%20%7D%0A%0A%20%20%20%20result%20%3D%20I3C_BusMasterSendCCC(master%2C%20%26amp%3BgetMRLCmd)%3B%0A%0A%20%20%20%20uint8_t%20*pData%20%3D%20getMRLCmd.data%3B%0A%20%20%20%20if%20((info-%26gt%3Bbcr%20%26amp%3B%20I3C_BUS_DEV_BCR_IBI_PAYLOAD_MASK)%20!%3D%200U)%0A%20%20%20%20%7B%0A%20%20%20%20%20%20%20%20info-%26gt%3BmaxIBILength%20%3D%20pData%5B2%5D%3B%0A%20%20%20%20%7D%0A%0A%20%20%20%20info-%26gt%3BmaxReadLength%20%3D%20(uint16_t)pData%5B0%5D%20%26lt%3B%26lt%3B%208UL%20%7C%20(uint16_t)pData%5B1%5D%3B%0A%0A%20%20%20%20free(getMRLCmd.data)%3B%0A%0A%20%20%20%20return%20result%3B%0A%7D%3C%2FCODE%3E%3C%2FPRE%3E%3CBR%20%2F%3E%3CP%3EThen%20we%20can%20%3CSPAN%3Ereproduce%20the%20stuck%20issue%20by%20calling%20them%3A%3C%2FSPAN%3E%3C%2FP%3E%3CPRE%20class%3D%22lia-code-sample%20language-cpp%22%3E%3CCODE%3Ei3c_device_information_t%20device_info%3B%0Amemset(%26amp%3Bdevice_info%2C%200%2C%20sizeof(device_info))%3B%0Adevice_info.dynamicAddr%20%3D%20icm42688p_sensorAddr%3B%0AI3C_BusMasterGetBCR(%26amp%3Bdemo_masterDev%2C%20%26amp%3Bdevice_info)%3B%0AI3C_BusMasterGetMaxReadLength(%26amp%3Bdemo_masterDev%2C%20%26amp%3Bdevice_info)%3B%3C%2FCODE%3E%3C%2FPRE%3E%3CP%3EAfter%20checking%20the%20waveform%2C%20we%20found%20that%20it%20gets%20stuck%20at%20GETMRL.%20After%20reading%20the%20MRL%20LSB%2C%20the%20SCL%20line%20stops%20and%20doesn't%20move%20anymore.%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22bell_huang_0-1744790912809.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22bell_huang_0-1744790912809.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F333410i8AAE9D0C5F579288%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22bell_huang_0-1744790912809.png%22%20alt%3D%22bell_huang_0-1744790912809.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CP%3EIn%20previous%20case%2C%20I3C_BusMasterGetBCR%20reads%20the%20BCR%20value%20of%20the%20ICM42688P%20as%2039%20(%3D%20b00100111)%2C%20which%20indicates%20that%20it%20supports%20BCR%5B2%5D%20IBI%20Payload.%20As%20a%20result%2C%20The%20dataSize%20of%20GETMRL%20in%20I3C_BusMasterGetMaxReadLength%20is%203.%3C%2FP%3E%3CBR%20%2F%3E%3CP%3EIf%20we%20assume%20that%20it%20does%20not%20support%20BCR%5B2%5D%20IBI%20Payload%2C%20that%20is%2C%20do%20not%20call%26nbsp%3BI3C_BusMasterGetBCR%2C%20then%26nbsp%3Bthe%20dataSize%20of%20GETMRL%20in%20I3C_BusMasterGetMaxReadLength%20is%202.%3C%2FP%3E%3CPRE%20class%3D%22lia-code-sample%20language-cpp%22%3E%3CCODE%3Ei3c_device_information_t%20device_info%3B%0Amemset(%26amp%3Bdevice_info%2C%200%2C%20sizeof(device_info))%3B%0Adevice_info.dynamicAddr%20%3D%20icm42688p_sensorAddr%3B%0A%2F%2FI3C_BusMasterGetBCR(%26amp%3Bdemo_masterDev%2C%20%26amp%3Bdevice_info)%3B%0AI3C_BusMasterGetMaxReadLength(%26amp%3Bdemo_masterDev%2C%20%26amp%3Bdevice_info)%3B%3C%2FCODE%3E%3C%2FPRE%3E%3CP%3EThen%20we%20can%20see%20GETMRL%20workable%2C%20it%20no%20longer%20gets%20stuck.%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22bell_huang_0-1744791335331.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22bell_huang_0-1744791335331.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F333414i38E8541E21E9240C%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22bell_huang_0-1744791335331.png%22%20alt%3D%22bell_huang_0-1744791335331.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CP%3EIn%20%3CA%20href%3D%22https%3A%2F%2Fwww.mipi.org%2Fmipi-i3c-basic-download%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EMIPI%20I3C%20Basic%E2%84%A0%20v1.1.1%3C%2FA%3E%26nbsp%3B%2C%26nbsp%3B5.1.9.3.6%20Set%2FGet%20Max%20Read%20Length%20(SETMRL%2FGETMRL)%2C%20the%203rd%20byte%20is%20IBI%20Payload%20Size%20which%20is%20optional.%20That%20is%2C%20if%20the%20sensor%20support%20IBI%20Payload%2C%20GETMRL%20shall%20read%203%20bytes.%20But%20in%20current%20SDK%2C%20it%20seems%20get%20stuck%20if%20we%20read%203%20bytes.%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22bell_huang_1-1744791750013.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22bell_huang_1-1744791750013.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F333417i87FF2B2D01CD6F21%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22bell_huang_1-1744791750013.png%22%20alt%3D%22bell_huang_1-1744791750013.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CBR%20%2F%3E%3CBR%20%2F%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2090840%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20LPC55S36%2C%20I3C%20GETMRL%20issue%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2090840%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EThanks.%20I%20tested%20IDE%20v24.12.148%20%26amp%3B%20SDK%26nbsp%3B%3CSPAN%3E25.03.00.%26nbsp%3B%3C%2FSPAN%3E%3CSPAN%3EThe%20GETMRL%20no%20longer%20get%20stuck.%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3ETest%20step%3A%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3E(1)%20Import%20SDK%20example(s)...%20-%26gt%3B%20driver_examples%20-%26gt%3B%20i3c%20-%26gt%3Bi3c_master_read_sensor_icm42688p%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3E(2)%20Remove%20source%2Fi3c_master_read_sensor_icm42688p.c%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3E(3)%20Add%20attached%26nbsp%3Bi3c_sensor_network.c%20to%26nbsp%3Bsource%2Fi3c_sensor_network.c%3C%2FSPAN%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2088022%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20LPC55S36%2C%20I3C%20GETMRL%20issue%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2088022%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F228396%22%20target%3D%22_blank%22%3E%40bell_huang%3C%2FA%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3EYou%20can%20download%20the%20latest%26nbsp%3B%2025.03.00%20SDK.%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22Harry_Zhang_0-1745823160002.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22Harry_Zhang_0-1745823160002.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F335125iE3A22E92ABC2D0C3%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22Harry_Zhang_0-1745823160002.png%22%20alt%3D%22Harry_Zhang_0-1745823160002.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E%22%3CSPAN%3EI%20think%20the%20best%20is%3A%20The%20GETMRL%20function%20returns%20fail%2Ferror%20status%20if%20the%20driver%20want%20to%20read%203%20bytes%20and%20the%20sensor%20doesn't%20support%203%20bytes%20(pull%20low%20the%20T-bit%20of%20LSB%20byte).%3C%2FSPAN%3E%22%3C%2FP%3E%0A%3CP%3EThank%20you%20for%20your%20suggestion.%20I%20will%20report%20it%20to%20the%20SDK%20team.%26nbsp%3BHope%20to%20improve%20in%20the%20future.%3C%2FP%3E%0A%3CP%3EBR%3C%2FP%3E%0A%3CP%3EHarry%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2088002%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20LPC55S36%2C%20I3C%20GETMRL%20issue%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2088002%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F229957%22%20target%3D%22_blank%22%3E%40Harry_Zhang%3C%2FA%3E%26nbsp%3B%2C%3C%2FP%3E%3CP%3EThanks%20for%20your%20test.%20Can%20you%20share%20the%20link%20of%26nbsp%3B%3CSPAN%3Elatest%20I3C%20driver%20file%20(MAKE_VERSION(2%2C%2013%2C%201))%3F%20I%20cannot%20find%20it%20out%20in%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fmcuxpresso.nxp.com%2Fen%2Fdashboard%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EMCUXpresso%20SDK%20Dashboard%3C%2FA%3E%26nbsp%3B.%20There%20are%20only%26nbsp%3B25.03.00%2C%26nbsp%3B2.16.000%2C%26nbsp%3B2.15.000.%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CP%3EI%20test%20LSM6DST%20which%20is%20an%20another%20sensor%20that%20supports%20GETMRL%203%20bytes.%20The%26nbsp%3Boriginal%20I3C%20driver%20doesn't%20lock.%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22bell_huang_0-1745820964321.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22bell_huang_0-1745820964321.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F335111i153215D78A5E54E9%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22bell_huang_0-1745820964321.png%22%20alt%3D%22bell_huang_0-1745820964321.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CP%3EIn%20comparison%2C%26nbsp%3B%3CSPAN%3EICM42688P%26nbsp%3Bpulls%20low%20the%20T-bit%20of%20LSB%20byte%20to%20indicate%20the%20end%20of%20the%20data.%20It%20means%20that%20if%20the%20sensor%20doesn't%20support%20GETMRL%203%20bytes%20and%20the%20original%20driver%20want%20to%20read%203%20bytes%2C%20then%20it%20will%20be%20locked.%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22bell_huang_1-1745821562842.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22bell_huang_1-1745821562842.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F335117i4F699CB75AD13544%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22bell_huang_1-1745821562842.png%22%20alt%3D%22bell_huang_1-1745821562842.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CP%3EI%20think%20the%20best%20is%3A%20The%20GETMRL%20function%20returns%20fail%2Ferror%20status%20if%20the%20driver%20want%20to%20read%203%20bytes%20and%20the%20sensor%20doesn't%20support%203%20bytes%20(pull%20low%20the%20T-bit%20of%20LSB%20byte).%3C%2FP%3E%3CP%3EHowever%2C%20it%20is%26nbsp%3Bacceptable%3A%20The%20GETMRL%20function%20will%20not%20lock%20at%20least.%3C%2FP%3E%3CBR%20%2F%3E%3CBR%20%2F%3E%3CBR%20%2F%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2087856%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20LPC55S36%2C%20I3C%20GETMRL%20issue%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2087856%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F228396%22%20target%3D%22_blank%22%3E%40bell_huang%3C%2FA%3E%3C%2FP%3E%0A%3CP%3EI%20am%20using%20the%20latest%20I3C%20driver%20file%20(MAKE_VERSION(2%2C%2013%2C%201))%2C%20and%20when%20the%20data%20size%20is%203%2C%20it%20no%20longer%20locks%20up.%20After%20confirming%20with%20the%20SDK%20team%2C%20there%20is%20indeed%20an%20update.%20So%20you%20can%20test%20it.%3CBR%20%2F%3EAlthough%20there%20is%20no%20lock%2C%20the%203rd%20byte%20is%20not%20received.%20After%20analysis%2C%20it%20appears%20that%20the%20slave%20actively%20terminated%20the%20read%20operation.%20So%20you%20can%20try%20to%20another%20sensor%20or%20consult%20the%20sensor%20manufacturer%20for%20further%20assistance.%3C%2FP%3E%0A%3CP%3EBR%3C%2FP%3E%0A%3CP%3EHarry%3C%2FP%3E%0A%3CBR%20%2F%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2084976%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20LPC55S36%2C%20I3C%20GETMRL%20issue%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2084976%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F228396%22%20target%3D%22_blank%22%3E%40bell_huang%3C%2FA%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3EYes%2C%20i%20can%20reproduce%20this%20issue%2C%26nbsp%3BI%20am%20investigating%20this%20issue.%3C%2FP%3E%0A%3CP%3EBR%3C%2FP%3E%0A%3CP%3EHarry%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2084968%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20LPC55S36%2C%20I3C%20GETMRL%20issue%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2084968%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F229957%22%20target%3D%22_blank%22%3E%40Harry_Zhang%3C%2FA%3E%26nbsp%3B%2C%3C%2FP%3E%3CP%3ECan%20you%20reproduce%20with%20attached%26nbsp%3Bi3c_sensor_network.c%20%3F%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2082889%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20LPC55S36%2C%20I3C%20GETMRL%20issue%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2082889%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F229957%22%20target%3D%22_blank%22%3E%40Harry_Zhang%3C%2FA%3E%20%2C%3C%2FP%3E%3CP%3E%3CSPAN%3EThis%20issue%20can%20be%20reproduced%20in%26nbsp%3B%3C%2FSPAN%3E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note-software%2FAN13577SW.zip%3F_gl%3D1*ev0hz5*_ga*MTY5MDA5MjI0LjE3NDQ3ODQ0NzY.*_ga_WM5LE0KMSH*MTc0NDkzOTM1My45LjEuMTc0NDkzOTM4MS4wLjAuMA..%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EBuilding%20an%20I3C%20Sensor%20Network%20Using%20LPC553x%2FLPC55S3x%3C%2FA%3E%3CSPAN%3E%26nbsp%3Bexample.%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2082508%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20LPC55S36%2C%20I3C%20GETMRL%20issue%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2082508%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F228396%22%20target%3D%22_blank%22%3E%40bell_huang%3C%2FA%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3EIn%20order%20to%20reproduce%20this%20issue%20quickly.%3C%2FP%3E%0A%3CP%3ECan%20you%20share%20the%26nbsp%3Bi3c_master_read_sensor_icm42688p.c%3F%3C%2FP%3E%0A%3CP%3EBR%3C%2FP%3E%0A%3CP%3EHarry%3C%2FP%3E%3C%2FLINGO-BODY%3E