LPC55S36-EVK and SDK flexspi examples

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55S36-EVK and SDK flexspi examples

跳至解决方案
903 次查看
jpholme
Contributor II

I can't make the FlexSPI Octal NOR flash examples work. When those examples tries to erase the flash, they report an error. Also, they cannot get a proper vendor ID. 

I have checked the jumpers several times; also accordign to the schematics of the EVK.

Is there anything to be aware of?

I'm using IAR EWARM and the SDK 2.16 examples.

0 项奖励
回复
1 解答
835 次查看
jpholme
Contributor II

Thanks! It was so nice that you tried it out and gave me the pictures. My mistake was that the JP44 and JP62 are oriented the opposite way as the other jumpers, so I got them connected between 2 and 3 instead. 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
836 次查看
jpholme
Contributor II

Thanks! It was so nice that you tried it out and gave me the pictures. My mistake was that the JP44 and JP62 are oriented the opposite way as the other jumpers, so I got them connected between 2 and 3 instead. 

0 项奖励
回复
862 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi

Please check the jumpers, i tested IAR EWARM and the SDK 2.16 FlexSPI Octal NOR flash examples, it can work.

Board settings
==============
Connect pin 1-2 of JP41,JP42,JP43,JP44,JP45,JP62,JP64 and JP65.
Close JP63,JP66,JP67,JP68 and JP69.

 

You can refer to my picture.

HangZhang_0-1728360897601.png

HangZhang_1-1728360965140.png

 

BR

Hang

 

0 项奖励
回复