LPC55S36-EVK and SDK flexspi examples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S36-EVK and SDK flexspi examples

Jump to solution
1,597 Views
jpholme
Contributor II

I can't make the FlexSPI Octal NOR flash examples work. When those examples tries to erase the flash, they report an error. Also, they cannot get a proper vendor ID. 

I have checked the jumpers several times; also accordign to the schematics of the EVK.

Is there anything to be aware of?

I'm using IAR EWARM and the SDK 2.16 examples.

0 Kudos
Reply
1 Solution
1,529 Views
jpholme
Contributor II

Thanks! It was so nice that you tried it out and gave me the pictures. My mistake was that the JP44 and JP62 are oriented the opposite way as the other jumpers, so I got them connected between 2 and 3 instead. 

View solution in original post

0 Kudos
Reply
2 Replies
1,530 Views
jpholme
Contributor II

Thanks! It was so nice that you tried it out and gave me the pictures. My mistake was that the JP44 and JP62 are oriented the opposite way as the other jumpers, so I got them connected between 2 and 3 instead. 

0 Kudos
Reply
1,556 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi

Please check the jumpers, i tested IAR EWARM and the SDK 2.16 FlexSPI Octal NOR flash examples, it can work.

Board settings
==============
Connect pin 1-2 of JP41,JP42,JP43,JP44,JP45,JP62,JP64 and JP65.
Close JP63,JP66,JP67,JP68 and JP69.

 

You can refer to my picture.

HangZhang_0-1728360897601.png

HangZhang_1-1728360965140.png

 

BR

Hang

 

0 Kudos
Reply