LPC55S16 - RAM backup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S16 - RAM backup

2,914件の閲覧回数
istvanmate
Contributor II

Is there a way to keep the RAM or some portion of it alive with a backup battery on the LPC55xx micro?

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,903件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Power Domain “Always On” includes PMC(Power management controller) and RTC.

This domain always has power as long as sufficient voltage is available on VBAT ([1.8 V –3.6 V]), that is external battery.

See below pic. "Always On " domain is in red. While RAM is not controlled by "Always On " domain. So we can't keep RAM with VBAT only.

ZhangJennie_0-1638542741826.png

Have a nice day,

Jun Zhang

0 件の賞賛
返信

2,886件の閲覧回数
istvanmate
Contributor II

Thanks for the quick reply.

It is what it is. I'll have to use external means to keep data alive between power cycles.

0 件の賞賛
返信

2,867件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome.

0 件の賞賛
返信