Hi,
According to https://www.nxp.com.cn/docs/zh/training-reference-material/TIP-NXP-MICROPROCESSOR-1.pdf
p.31,
LPC55S16 supports
"Keyboard:✓ Enabled unique EZH HW accelerator for up to 128 (8*16) key scan."
Where to find the sample code and document for this HW keypad usage for LPC55S16?
已解决! 转到解答。
Hi
LPC55S16 doesn't have keypad. Technically EZH can emulate it but we don't have demo code.
The demo is under SDK.
Have a nice day,
Jun Zhang
在原帖中查看解决方案
Hello,
As per my knowledge, you can find sample code and documentation for using the Keypad Port (KPP) on the LPC55S16 microcontroller:
HI @felix1
We don't have EZH Keypad demo code.
We only have rotary encoder ezh demo application which is included in MCUXpresso SDK .
rotary_encoder_ezh
Hope this will help you,
1) Can you classify LPC55S16 have Keypad Port (KPP) HW like RT1050 MCU or not?
I can not find KPP section in LPC55S16 datasheet.
2) The example "rotary_encoder_ezh" in which directory of the LPC SDK?
I can not find this LPC example.
I can not find this example in SDK 2.9.1, can you check it?
This demo exists on my side.
When download, please select "all toolchains" and "select all". check again
Thanks,
The example "rotary_encoder_ezh" is not in SDK 2.14.0, it seems just in SDK 2.9.1 and keil project type only.
Hi felix1
Yes, you are right. rotary_encoder_ezh is not included in SDK2.14 for LPCXpresso55S16. But it is included in SDK2.14 for LPCXpresso55S69