LPC55S16 - CANOpen Autostart?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S16 - CANOpen Autostart?

1,542 次查看
JK_265
Contributor III

Using LPC55S16 with CANOpen stack from ESA as provided by MCUXpresso.
Per the documentation, if I modify the file nodecfg.h so that AUTOSTART is defined as 1 instead of 0, then my node should automatically enter the CANOpen operational state.  I have tried this, but after reset the node is still pre-operational.  Can anyone help?

Thanks!

0 项奖励
回复
2 回复数

1,527 次查看
JK_265
Contributor III

I just noticed these comments at the top of the nodecfg file:

/*
* Note: All settings below are for informational purposes only and
* must not be changed in projects that use the NXP SDK library
* version of MicroCANopen. Changes here will not affect the
* delivered library and may lead to applications that fail to
* build or perform.
*/

So, does that mean I am out of luck, because NXP delivers the precompiled CANOpen library and I can't rebuild it?

 

0 项奖励
回复

1,498 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @JK_265 

Yes, according to this Note message, this is a precompiled CANOpen library.

Hope this will help you.

BR

Hang

0 项奖励
回复