Inquiry About USB Connectivity and Verification for LPC11C24F Microcontroller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Inquiry About USB Connectivity and Verification for LPC11C24F Microcontroller

735 次查看
Sumedha
Contributor I

Greetings,

I am Sumedha, and I am from Continental Automotive Singapore Pte Ltd.

I am presently working on a project with the LPC11C24F microcontroller. I managed to utilize a USB to UART cable and the respective pins 47 (TX), 46 (RX), and 41 (Ground) successfully. Is there a specific command or method to check if the USB connection has been successfully made?  Can you suggest a way to check if the USB connection has been properly set up? I have been facing a problem for the past week in confirming the connection status. Furthermore, I would be grateful for any suggestions on USB to UART cables that NXP would support for use with the LPC11C24F.One more issue that is encountered would be sometimes I encounter garbage values for certain Baud Rate but sometimes there is no garbage value detected. Secondly when i power up the board how many LED's are specifically turned on.

Thank you so much for backing me up. I am eagerly anticipating your prompt response.

Warm regards,
Sumedha Putta

Product Cybersecurity & Privacy Office

Automotive Technology 

Software and Central Technologies – Architecture & Software

Bill/Visitor Address:

 

Continental Automotive Singapore Pte Ltd

Continental Building, 80 Boon Keng Road,

Singapore 339780  

 

 

Email :   [email protected]

Web   :   www.continental-automotive.com

 

Sumedha_0-1718961623479.jpeg

 

 

 

0 项奖励
回复
0 回复数