LPC55S16 - ADC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55S16 - ADC

跳至解决方案
4,415 次查看
Dhaya
Contributor III

Hi,

    I'm using LPC55S16 (100 pin package) and configured the ADC in 16-bit resolution. While reading the value, ADC value get oscillated more. How I can reduce the oscillation?. Even if i used average of 50, it gets oscillated. Kindy resolve it, if it is possible

0 项奖励
回复
1 解答
4,363 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the spec of ADC of LPC5516,the ENOB is 12.1 bits in 16 bits resolution and single-ended mode, in other words, the low 4 bits is random, the random value is 16 LSB.

But you said that the Oscillating of value for current and previous value is about +/-80 LSB, it is too big, can you share the analog circuit and external analog source impedance?

BR

XiangJun Rong

 

xiangjun_rong_0-1697612855843.png

 

在原帖中查看解决方案

3 回复数
4,401 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you explain what the ADC sampling results oscillation is? If you sample a DC voltage, does the ADC sampling results oscillate? or just the low 3 bits oscillate for every ADC results.

BR

XiangJun Rong

4,387 次查看
Dhaya
Contributor III

Hi @xiangjun_rong ,

            Here we used DC voltage samplings (max. 3.3V) and taken average of 50. Oscillating of value for current and previous value is about +/-80. We used it to verify linear POT which datasheet is attached here

0 项奖励
回复
4,364 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the spec of ADC of LPC5516,the ENOB is 12.1 bits in 16 bits resolution and single-ended mode, in other words, the low 4 bits is random, the random value is 16 LSB.

But you said that the Oscillating of value for current and previous value is about +/-80 LSB, it is too big, can you share the analog circuit and external analog source impedance?

BR

XiangJun Rong

 

xiangjun_rong_0-1697612855843.png