LPC55S16 2nd stage bootloader with Secure Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S16 2nd stage bootloader with Secure Boot

1,393 Views
evgreen
Contributor I

Hello,

I am looking for a Secure Boot 2nd stage bootloader for LPC55S16.

On the LPC55S1x NXP web page, is listed the AN12327 application note for the implementation of a 2nd stage bootloader, but this bootloader doesn't include flashing Secure Boot firmware, only flashing a plain firmware received by UART.

Is possible to have such a 2nd stage bootloader with Secure Boot on LPC55S16? if so, can you please point me to some example or explain how to implement it?

1 Reply

1,332 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @evgreen 

Sorry there isn't second bootloader with secure boot so far. 

If you want to use secure boot, recommend enable secure boot function to use the secure bootloader inside BOOT ROM.

 

BR

Alice