LPC55S06x_Evk_Board Flashing Error while running at 96MHZ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S06x_Evk_Board Flashing Error while running at 96MHZ

2,125 Views
nagaprasadvasam
Contributor III

Dear all,

we are working on LPC controller(LPC55s06x),tried to generate clock at 96Mhz with reference code using configuration as follows,
PDRUNCFGCLR0 = 1 << 5;

/* setting the FRO clock for 12mhz */
SYSCON_PRESETCTRLCLR2 = (1 << 27);
SYSCON_AHBCLKCTRLSET2 = 0x8000000U;
PDRUNCFGCLR0 = 1 << 5;
FRO192M_CTRL |= ((1 << 14) & 0x4000 );
SYSCON_MAINCLKSELA = 0x00;

/* setting the FRO clock for 96mhz */
SYSCON_PRESETCTRLCLR2 = (1 << 27);
SYSCON_AHBCLKCTRLSET2 = 0x8000000U;
PDRUNCFGCLR0 = 1 << 5;
FRO192M_CTRL |= ((1 << 30) & 0x40000000U );

/* Power manager voltage selection */
DCDC0 = 0x01C05CF8;
DCDC1 = 0x010E6E75;

/* flash configuration */
INTCLRSTATUS = 0x1F;
DATAW[0] = ((DATAW[0] & 0xFFFFFFFF) | (7 & (0xF000U >> 12)));
CMD = 0x02;
while((INT_STATUS & 4) == 0);
FMCCR = (FMCCR & ~(0xF000U)) | ((0 << 12) & 0xF000U)

SYSCON_MAINCLKSELA = 0x03;
SYSCON_MAINCLKSELA = 0x00;
SYSCON_AHBCLKDIV = 0x00;
we have tried to flash code to controller through CMSIS DAP.getting error as Fatal erro:Failed to connect to cpu.even though if we tried reset eval board then also not able to flash from next time also tried to flash using JTAG/I-jet debuggers as per pin configuration provided in schematics, then also not able to flash controller.

Please help us to resolve this issue.

best regards,

NagaPrasad.

Labels (4)
0 Kudos
Reply
1 Reply

2,087 Views
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @nagaprasadvasam 

 

I would like to apologize for the delay. I got sick suddenly and couldn't write a response to you.

 

Regarding your issue, it is my pleasure to help you with your concern, but firstly, may you tell me if you are using your custom board or a development board for LPC?
Also as a question, were you able sometime before to flash that mcu? Did you try flashing a simple led blinky code to your mcu?

 

I will stay tune to your response, so I can help you with it. Please let me know if you have more questions.

 

Thank you so much.

Sincerely,

Pablo Avalos.

0 Kudos
Reply