LPC556X BGA Package ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC556X BGA Package ?

Jump to solution
2,662 Views
tilakmarupilla
Contributor II

Hello all,


In Data sheets of LPC556X Microcontroller, VFBGA98 packages are seen. Contrary to that, there are no BGA options to buy. Only LQFP are there.

Can I know when will this VFGA package will be available ?

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
2,553 Views
soledad
NXP Employee
NXP Employee

Hello Tilak,

IT is correct the LPC55S6x family it is going to have a VBGA98 package available in Q32019, If you need the device earlier please contact your local NXP Sales, they would be able to help you.

Best Regards,

TIC

View solution in original post

2 Replies
2,554 Views
soledad
NXP Employee
NXP Employee

Hello Tilak,

IT is correct the LPC55S6x family it is going to have a VBGA98 package available in Q32019, If you need the device earlier please contact your local NXP Sales, they would be able to help you.

Best Regards,

TIC

2,553 Views
tilakmarupilla
Contributor II

Thanks for the confirmation

0 Kudos
Reply