LPC556X BGA Package ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC556X BGA Package ?

ソリューションへジャンプ
2,684件の閲覧回数
tilakmarupilla
Contributor II

Hello all,


In Data sheets of LPC556X Microcontroller, VFBGA98 packages are seen. Contrary to that, there are no BGA options to buy. Only LQFP are there.

Can I know when will this VFGA package will be available ?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
2,575件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Tilak,

IT is correct the LPC55S6x family it is going to have a VBGA98 package available in Q32019, If you need the device earlier please contact your local NXP Sales, they would be able to help you.

Best Regards,

TIC

元の投稿で解決策を見る

2 返答(返信)
2,576件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Tilak,

IT is correct the LPC55S6x family it is going to have a VBGA98 package available in Q32019, If you need the device earlier please contact your local NXP Sales, they would be able to help you.

Best Regards,

TIC

2,575件の閲覧回数
tilakmarupilla
Contributor II

Thanks for the confirmation

0 件の賞賛
返信