LPC556X BGA Package ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC556X BGA Package ?

跳至解决方案
2,745 次查看
tilakmarupilla
Contributor II

Hello all,


In Data sheets of LPC556X Microcontroller, VFBGA98 packages are seen. Contrary to that, there are no BGA options to buy. Only LQFP are there.

Can I know when will this VFGA package will be available ?

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
2,636 次查看
soledad
NXP Employee
NXP Employee

Hello Tilak,

IT is correct the LPC55S6x family it is going to have a VBGA98 package available in Q32019, If you need the device earlier please contact your local NXP Sales, they would be able to help you.

Best Regards,

TIC

在原帖中查看解决方案

2 回复数
2,637 次查看
soledad
NXP Employee
NXP Employee

Hello Tilak,

IT is correct the LPC55S6x family it is going to have a VBGA98 package available in Q32019, If you need the device earlier please contact your local NXP Sales, they would be able to help you.

Best Regards,

TIC

2,636 次查看
tilakmarupilla
Contributor II

Thanks for the confirmation

0 项奖励
回复