LPC553x tADCSTUP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC553x tADCSTUP

Jump to solution
2,666 Views
Bela1
Contributor III

Ladies and Gentlemen,

I am studying the datasheet (LPC553x Product data sheet, Rev. 5.0 – 7. March 2024) and the Reference Manual (LPC553x Reference Manual, Rev. 3, 07/2023) of LPC3356JBD100. This is the chip I am planning to use.

There’s a parameter I cannot find. It is: tADCSTUP. It must be known because it is necessary for properly setting the ADC up.

However, google has found something in the datasheet of LPC55S6x Product data sheet (Rev. 2.4 — 8 December 2022), Table 12.2, page 105, there’s a tADCSTUP parameter, it is 5usec.

Is this 5usec also true for LPC5536JBD100?

How can I find the proper parameter for my chip?

Thank You in advance.

0 Kudos
Reply
1 Solution
2,571 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, thanks for your waiting I have confirmed with the internal department, that the tADCSTUP value is 5us in LPC553x.

Best regards,
Pavel

View solution in original post

0 Kudos
Reply
6 Replies
2,572 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, thanks for your waiting I have confirmed with the internal department, that the tADCSTUP value is 5us in LPC553x.

Best regards,
Pavel

0 Kudos
Reply
2,564 Views
Bela1
Contributor III

Thank You Pavel, everything seems to be clear now.

You can close this issue, thanks for the help.

0 Kudos
Reply
2,622 Views
Bela1
Contributor III

Hallo Pavel,

things are getting clear now. As I understand, signal SWO may not be either on PIO0_8 or on PIO0_18 at the time of reset, the uC can be reprogrammed and debugged without this signal. It's OK.

The signals Tracedata0 ..Tracedata3 and TraceCLK are also not absolutely necessary, they can be used as regular I/O.

I will route my board accordingly, and I do hope it will perform well. Thank You for the help.

0 Kudos
Reply
2,651 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, let me get into your case and when I have more information, I will contact you.

Best regards,
Pavel

0 Kudos
Reply
2,645 Views
Bela1
Contributor III

Hallo Pavel,

thank You in advance for Your support. At the moment - since a few days - I am digging myself into the HW development with the microcontroller LPC5536JBD100. The environment I will use: MCUXpresso IDE, MCU-LINK PRO and my own HW board with LPC5536JBD100. To begin the FW development I also have an LPC5536-EVK but I do not plan long time with this evalboard, just until my own HW arrives. All the HW are recently purchased, and all the SW tools are new installed.

I have more than one question, all regarding LPC5536JBD100. Let me go just one by one.

The first one is: where can I find the parameter tADCSTUP? I cannot find it in the datasheet (LPC553x Product data sheet, Rev. 5.0, 7. March 2024 is what I have).

This parameter defines, how long is the minimum time, one has to wait after switching the ADC ON. It is necessary for the internal analog signals to set their final value. My opinion is, this parameter must be in Table 46 (Page 124-125) but it isn't there and I don't find it anywhere else.

 

Question two: I am a bit confused, due to the connection of SWD signals. I do have the AN13707 and the datasheet, and NXP's MCUXpresso Config tool, V15.0, too.

Signal SWO is routed to PIO0_8 and also to PIO0_18. Which one is best to use? The debugger must work right at the very first power-up, because the first FW must be somehow downloaded into the processor.

Question three: How can I use the Tracedata signals? I don't see any example neither in datasheet, in RefManual or in appnotes, too. Aren't they necessary for debugging?

 

0 Kudos
Reply
2,631 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I´m asking the internal department the first question I noticed the same the time analog is missing. 

for the other 2 questions about the SWO, there is nothing special.

Pavel_Hernandez_0-1711503789526.pngPavel_Hernandez_0-1711503789526.png

But if you want to use it for other purposes maybe this could interest you, the PIO8 (2) and PIO18 (4).

Pavel_Hernandez_1-1711503867506.pngPavel_Hernandez_1-1711503867506.png

Let me get more information from the last question.

Best regards,
Pavel

0 Kudos
Reply