LPC553x I3C PUR Signal availability

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC553x I3C PUR Signal availability

跳至解决方案
615 次查看
mf89
Contributor I

Hi,

the LPC553x MCU Features a Hardware I3C Peripheral. Is the "PUR" Pull Up resistor control Pin only available in the 100 Pin Package ?

 

If yes is there an alternative solution for the 64 and 48 Pin Package to handle external Pull Ups on SDA line ?

标签 (1)
0 项奖励
回复
1 解答
608 次查看
Dezheng_Tang
NXP Employee
NXP Employee

Yes, only 100-pin package has PUR pin on external SDA pull-up, for smaller package, you have to configure a pin as GPIO and toggle it to control the external SDA pull-up. It's meant for a strong pull-up, not sure if it's always needed depending on your application. 

在原帖中查看解决方案

0 项奖励
回复
1 回复
609 次查看
Dezheng_Tang
NXP Employee
NXP Employee

Yes, only 100-pin package has PUR pin on external SDA pull-up, for smaller package, you have to configure a pin as GPIO and toggle it to control the external SDA pull-up. It's meant for a strong pull-up, not sure if it's always needed depending on your application. 

0 项奖励
回复