LPC553x I3C PUR Signal availability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC553x I3C PUR Signal availability

ソリューションへジャンプ
734件の閲覧回数
mf89
Contributor I

Hi,

the LPC553x MCU Features a Hardware I3C Peripheral. Is the "PUR" Pull Up resistor control Pin only available in the 100 Pin Package ?

 

If yes is there an alternative solution for the 64 and 48 Pin Package to handle external Pull Ups on SDA line ?

ラベル(1)
0 件の賞賛
返信
1 解決策
727件の閲覧回数
Dezheng_Tang
NXP Employee
NXP Employee

Yes, only 100-pin package has PUR pin on external SDA pull-up, for smaller package, you have to configure a pin as GPIO and toggle it to control the external SDA pull-up. It's meant for a strong pull-up, not sure if it's always needed depending on your application. 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
728件の閲覧回数
Dezheng_Tang
NXP Employee
NXP Employee

Yes, only 100-pin package has PUR pin on external SDA pull-up, for smaller package, you have to configure a pin as GPIO and toggle it to control the external SDA pull-up. It's meant for a strong pull-up, not sure if it's always needed depending on your application. 

0 件の賞賛
返信