LPC5536 I3C NO WORK----USE LPC55S36 SAMPLE CODE I3C SENSOR NET WORK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5536 I3C NO WORK----USE LPC55S36 SAMPLE CODE I3C SENSOR NET WORK

ソリューションへジャンプ
6,589件の閲覧回数
luna_liang
Contributor II

DEARS,

I used LPCXpresso55S36 test i3c port,use i3c port PIN 69,PIN 55, no clock and data.please help check if the demo is OK,or please help share a project about I3C TO USB application ,thank you.

luna_liang_0-1710315891456.png

 

0 件の賞賛
返信
1 解決策
6,568件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @luna_liang 

I downloaded SDK_2_10_2_LPCXpresso55S36, and run the i3C master_read_sensor_icm42688p example. It can work.

Please note the readme in the example.

Image (6).jpg

I hope can help you.

Best regards,
Hang

 

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
6,569件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @luna_liang 

I downloaded SDK_2_10_2_LPCXpresso55S36, and run the i3C master_read_sensor_icm42688p example. It can work.

Please note the readme in the example.

Image (6).jpg

I hope can help you.

Best regards,
Hang

 

0 件の賞賛
返信
6,557件の閲覧回数
luna_liang
Contributor II

now download is 2_15 ,please help share 2_10 SDK,thank you.

タグ(1)
0 件の賞賛
返信
6,557件の閲覧回数
luna_liang
Contributor II
现在下载的都是2_15版本的例程,能分享你的2_10吗
0 件の賞賛
返信
6,555件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @luna_liang 

您好,

请您在官网如图选择2.10 SDK 下载。

HangZhang_0-1710404437852.png

谢谢

 

0 件の賞賛
返信
6,525件の閲覧回数
luna_liang
Contributor II

麻烦给一下您邮箱,thank you。

0 件の賞賛
返信
6,528件の閲覧回数
luna_liang
Contributor II

luna_liang_0-1710469173264.png

2.10.2这个工程只有这个工程,选项里有I2C,没看到I3C module

这个是可以用吗

0 件の賞賛
返信
6,515件の閲覧回数
luna_liang
Contributor II

dear hang,

thank you,my demo has no R554,had read the read me doc,this need a short connect in R554_ PIN 2 TO PIN3,

SO can not run sussesful . 

only to print: I3C master do dynamic address assignmentto the sensor slave.

0 件の賞賛
返信
6,483件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi @luna_liang 

You can download the 2.10.2 SDK by following the steps in the video.

Best regards, Alex

0 件の賞賛
返信
6,495件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @luna_liang

你下载的应该是2.15的SDK,2.10的里面没有R554。

 下图为下载的压缩包,和 read me。我会邮箱发给你该压缩包。

HangZhang_0-1710490930227.pngHangZhang_1-1710490979233.png

 

0 件の賞賛
返信