DEARS,
I used LPCXpresso55S36 test i3c port,use i3c port PIN 69,PIN 55, no clock and data.please help check if the demo is OK,or please help share a project about I3C TO USB application ,thank you.
解決済! 解決策の投稿を見る。
Hi @luna_liang
I downloaded SDK_2_10_2_LPCXpresso55S36, and run the i3C master_read_sensor_icm42688p example. It can work.
Please note the readme in the example.
I hope can help you.
Best regards,Hang
元の投稿で解決策を見る
now download is 2_15 ,please help share 2_10 SDK,thank you.
您好,
请您在官网如图选择2.10 SDK 下载。
谢谢
麻烦给一下您邮箱,thank you。
2.10.2这个工程只有这个工程,选项里有I2C,没看到I3C module
这个是可以用吗
dear hang,
thank you,my demo has no R554,had read the read me doc,this need a short connect in R554_ PIN 2 TO PIN3,
SO can not run sussesful .
only to print: I3C master do dynamic address assignmentto the sensor slave.
You can download the 2.10.2 SDK by following the steps in the video.
Best regards, Alex
你下载的应该是2.15的SDK,2.10的里面没有R554。
下图为下载的压缩包,和 read me。我会邮箱发给你该压缩包。