LPC5536 CRP Level and SWD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5536 CRP Level and SWD

1,218 Views
SilentBob
Contributor I

Hello experts,

The processor LPC5536 supports 5 different CRP levels, which are not re-settable. For example, with a CRP level of 2, can I still erase the flash and update the program via SWD?

SilentBob_0-1667812884366.png

 

Thanks for the help in advance

 

0 Kudos
Reply
1 Reply

1,196 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @SilentBob 

With the CRP you still are able to erase the flash memory, if you want to erase it, you could refer to the Application note "Building an I3C Network using LPC553x/LPC55S3x" section 4.3.1. You can find the application note in this link.

Let me know if you have any other question.

Best Regards, Miguel.

0 Kudos
Reply