LPC5536 CRP Level and SWD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5536 CRP Level and SWD

1,240件の閲覧回数
SilentBob
Contributor I

Hello experts,

The processor LPC5536 supports 5 different CRP levels, which are not re-settable. For example, with a CRP level of 2, can I still erase the flash and update the program via SWD?

SilentBob_0-1667812884366.png

 

Thanks for the help in advance

 

0 件の賞賛
返信
1 返信

1,218件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @SilentBob 

With the CRP you still are able to erase the flash memory, if you want to erase it, you could refer to the Application note "Building an I3C Network using LPC553x/LPC55S3x" section 4.3.1. You can find the application note in this link.

Let me know if you have any other question.

Best Regards, Miguel.

0 件の賞賛
返信