LPC5528: Minimum operating frequency external crystal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5528: Minimum operating frequency external crystal

ソリューションへジャンプ
3,319件の閲覧回数
airios_arno
Contributor II

We are designing a new product with the LPC5528JBD64 and noticed a discrepancy in the product datasheet (revision 2.0), regarding the minimum operating frequency of the external crystal oscillator.

On page 4, under Clock generation, it mentions a range of 12 MHz to 32 MHz.

However, in chapter 7.19.1 Clock sources, a range of 1 MHz to 32 MHz is specified.

The MCUXpresso Clock Config tool also expects me to enter at least 12 MHz, but that might have been based off of incorrect data as well.

Can someone from NXP maybe give me a definitive answer on what the minimum operating frequency for the external crystal oscillator is?

Thanks,
Arno

PS: I also noticed that there is a discrepancy with regards to the external clock input (25 MHz on page 4 and 24 MHz in the aforementioned chapter).

0 件の賞賛
返信
1 解決策
3,290件の閲覧回数
arno1
Contributor II

One of our suppliers also contacted NXP regarding this issue and just reported back to us:
- For an external clock source the frequency range is 1 MHz - 24 MHz.
- For an external crystal oscillator the frequency range is 12 MHz - 32 MHz.

元の投稿で解決策を見る

3 返答(返信)
3,291件の閲覧回数
arno1
Contributor II

One of our suppliers also contacted NXP regarding this issue and just reported back to us:
- For an external clock source the frequency range is 1 MHz - 24 MHz.
- For an external crystal oscillator the frequency range is 12 MHz - 32 MHz.

3,313件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Arno,

I have checked the data sheet of LPC5528, there is a discrepancy for the minimum crystal frequency exactly, one part says the minimum crystal frequency is 1MHz, another part says it is 12mhz.

Anyway, I have asked the design team, I will answer you after I get feedback.

BR

XiangJun Rong

0 件の賞賛
返信
3,287件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Arno,

This is feedback from AE team, hope it can help you.

"

 For an external clock source, the frequency range is 1 MHz - 24 MHz. - For an external crystal oscillator the frequency range is 12 MHz - 32 MHz.

"

We will update the data sheet of LPC5528 later.

BR

XiangJun Rong