LPC5528 JTAG circuit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,546件の閲覧回数
yuto
Contributor I

Hi.

Can you tell me about JTAG on the LPC5528?
Is writing programs in JTAG supported?
If so, please tell me about the schematic connections.

Preferred usage
Program writing in JTAG
Debugging with SWD
Write the program at SPI during ISP Boot

image.png

 

ラベル(1)
0 件の賞賛
返信
1 解決策
3,515件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

We use SWD and debug and program.

ISP boot code is in boot ROM, user can't reprogram boot ROM

元の投稿で解決策を見る

4 返答(返信)
3,534件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi yuto

Here is a very classic article for JTAG/SWD design

https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44

 

Note that, for LPC5528, JTAG is used on this device for boundary scan and production test ONLY and
cannot to used for debugging purposes.

 

Have a nice day,

Jun Zhang

0 件の賞賛
返信
3,526件の閲覧回数
yuto
Contributor I

Thank you, Jun Zhang, for your reply!

Tell me more.

>"JTAG is used on this device for boundary scan and production test ONLY"

Flash Programming in JTAG is not possible?

How to programming the firmware you have created is ISP boot?
(UART,SPI,USB,etc..)

0 件の賞賛
返信
3,516件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

We use SWD and debug and program.

ISP boot code is in boot ROM, user can't reprogram boot ROM

3,508件の閲覧回数
yuto
Contributor I

Thank you, Jun Zhang, for your reply!

I understand.

0 件の賞賛
返信