LPC5528 JTAG circuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5528 JTAG circuit

Jump to solution
3,510 Views
yuto
Contributor I

Hi.

Can you tell me about JTAG on the LPC5528?
Is writing programs in JTAG supported?
If so, please tell me about the schematic connections.

Preferred usage
Program writing in JTAG
Debugging with SWD
Write the program at SPI during ISP Boot

image.pngimage.png

Labels (1)
0 Kudos
Reply
1 Solution
3,479 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

We use SWD and debug and program.

ISP boot code is in boot ROM, user can't reprogram boot ROM

View solution in original post

4 Replies
3,498 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi yuto

Here is a very classic article for JTAG/SWD design

https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44

 

Note that, for LPC5528, JTAG is used on this device for boundary scan and production test ONLY and
cannot to used for debugging purposes.

 

Have a nice day,

Jun Zhang

0 Kudos
Reply
3,490 Views
yuto
Contributor I

Thank you, Jun Zhang, for your reply!

Tell me more.

>"JTAG is used on this device for boundary scan and production test ONLY"

Flash Programming in JTAG is not possible?

How to programming the firmware you have created is ISP boot?
(UART,SPI,USB,etc..)

0 Kudos
Reply
3,480 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

We use SWD and debug and program.

ISP boot code is in boot ROM, user can't reprogram boot ROM

3,472 Views
yuto
Contributor I

Thank you, Jun Zhang, for your reply!

I understand.

0 Kudos
Reply