LPC5506 ADC reference voltage source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5506 ADC reference voltage source

1,708 Views
ryanlush
Contributor IV

I've been given some hardware that has VDDA tied to VREFP but left to float on a 100nF capacitor. When I try to read the internal temperature sensor on CH26 I get 0. I loaded the lpadc-temperature-measurement example on my hardware and also got 0. When looking at the reference manual for this chip I don't see an option for an internal reference voltage. Is this true? Is there a way for me to use the ADC without an external reference? Most of our products use the ADC to measure something external so the reference voltage gets tied to something.

0 Kudos
Reply
2 Replies

1,691 Views
ryanlush
Contributor IV
After tying VDDA (pin 6) & VREFP (pin 7) to VDD (pin 5) I got the reading I would expect. Is this my only solution?
0 Kudos
Reply

1,687 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

It is needed an external voltage references to perform the SAR ADC. You can choose between VREFP or VDDA.

_Leo__0-1715278634583.png_Leo__0-1715278634583.png

Hope it helps you.

Have a nice day!

0 Kudos
Reply