LPC5504 FLASH READ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5504 FLASH READ

1,241 Views
jacklin_123
Contributor I

jacklin_123_0-1716953217747.pngjacklin_123_0-1716953217747.pngjacklin_123_1-1716953231105.pngjacklin_123_1-1716953231105.png

FLASH RANGE :0X0 - 0X20000

if i read the value of this address, The program will enter the HardFault interrupt function.

Every other chip I've ever used can read the data, as long as its address is in flash range

Why is LPC5504 an exception.

Has anyone come across it? Please help me. Thank you

 

0 Kudos
Reply
1 Reply

1,222 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @jacklin_123 

May I ask if you have erased the flash and read it directly?

If so, please refer to this.

[LPC55xx] How to fix AHB Read HardFault Error - NXP Community

Hope this will help you.

BR

Hang

0 Kudos
Reply