LPC5500 Benchmark.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5500 Benchmark.

1,796件の閲覧回数
arimendes
Contributor III

The LPC55S69 benchmark running out of SRAMX is 4.02 and running out of internal flash is only 2.333.

Comparing with the STM32L5: SRAM 4.02 and Flash 3.97. 

I suppose the new high performance LPC557x and LPC558x (180MHZ) series will have some kind of Flash accelerator or cache. Correct? 

When the ducumentation for this new series will be available? 

ラベル(1)
0 件の賞賛
返信
1 返信

1,700件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ari Mendes,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) I suppose the new high-performance LPC557x and LPC558x (180MHZ) series will have some kind of Flash accelerator or cache. Correct?
-- Yes.
2) When the documentation for this new series will be available?
-- The exact launch or release schedule has not been determined, however,  as I know, they definitely won't be delayed to the end of Q2 in 2020.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信