LPC54xxx GPIO is powered earlier than VDD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54xxx GPIO is powered earlier than VDD

1,166 次查看
hiwave
NXP Employee
NXP Employee

Hi, 

Customer is using LPC54016,  one IO pin is used to monitor the power supply state, which will be powered 160us earlier  than LPC54016 VDD,  can this result MCU power up failure?  or  is it potential risk? 

Does LPC54xxx have some limitations for power on? 

Thanks!    

Best Regards

Derek 

标签 (1)
0 项奖励
回复
1 回复

1,080 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Derek,

As you know that the digital pin has ESD protection circuit, if you can limit the current of the I/O pin to 2mA even if the VDD is not powered, it is okay. In other words, it is okay if you connect a serial resistor to limit the current to less than 2mA.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复