LPC54xxx GPIO is powered earlier than VDD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54xxx GPIO is powered earlier than VDD

435 Views
hiwave
NXP Employee
NXP Employee

Hi, 

Customer is using LPC54016,  one IO pin is used to monitor the power supply state, which will be powered 160us earlier  than LPC54016 VDD,  can this result MCU power up failure?  or  is it potential risk? 

Does LPC54xxx have some limitations for power on? 

Thanks!    

Best Regards

Derek 

Labels (1)
0 Kudos
1 Reply

349 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Derek,

As you know that the digital pin has ESD protection circuit, if you can limit the current of the I/O pin to 2mA even if the VDD is not powered, it is okay. In other words, it is okay if you connect a serial resistor to limit the current to less than 2mA.

Hope it can help you

BR

XiangJun Rong

0 Kudos