LPC54xx The maximum frequency for the SCTimer/PWM clock is 100 MHz ??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC54xx The maximum frequency for the SCTimer/PWM clock is 100 MHz ??

跳至解决方案
2,672 次查看
ZhaiYF
Contributor I

 

ZhaiYF_1-1640313406653.png

Question 1、
In the figure  "The maximum frequency for the SCTimer/PWM clock is 100 MHz."
Is it only applicable for clock after SCTCLKSEL ?

Question 2、
If set CLKMODE=0 in SCTimer/PWM configuration register。Is there maximum frequency
limit for system clock ?

 

0 项奖励
回复
1 解答
2,627 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi ZhaiYF 

There are two type of input for SCT, the the 100MHz clock limitation is only valid for the clock source inputted from external pads (SCT_IN7), if you use system clock as the SCTimer/PWM clock source, the system clock frequency can be greater than 100MHz.

ZhangJennie_0-1640610687604.png

You can also see this "Remarks "  immediately below "Select a function clock using SCTCLKSEL (Section 7.5.41)."

ZhangJennie_1-1640610889410.png

Hope this helps,

Jun Zhang

 

 

在原帖中查看解决方案

3 回复数
2,649 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI ZhaiYF 

The Maximum freq for SCT is 100Mhz. any input freq. beyond this value is an invalided input and will have un-guaranteed behavior. also , the 100Mhz limit is mainly com from pad limitation. not the SCT module itself

Have a nice day, 

Jun Zhang

0 项奖励
回复
2,636 次查看
ZhaiYF
Contributor I

HI Jun Zhang

Thanks.

Maybe I confused the SCTimer clock source and clock input. 

Now, SCTimer does not need any external clock input except the system clock. I want to Confirm whether the SCTimer module can work stably if the system clock is greater than 100MHz, such as 180MHz.

The MCU used is lpc54618.

0 项奖励
回复
2,628 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi ZhaiYF 

There are two type of input for SCT, the the 100MHz clock limitation is only valid for the clock source inputted from external pads (SCT_IN7), if you use system clock as the SCTimer/PWM clock source, the system clock frequency can be greater than 100MHz.

ZhangJennie_0-1640610687604.png

You can also see this "Remarks "  immediately below "Select a function clock using SCTCLKSEL (Section 7.5.41)."

ZhangJennie_1-1640610889410.png

Hope this helps,

Jun Zhang