LPC54S018M: SWD's SWDIO and SWCLK pins pullup/pulldown

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54S018M: SWD's SWDIO and SWCLK pins pullup/pulldown

Jump to solution
3,600 Views
belmontbob59
Contributor IV

KEIL recommends to add pull up on SWDIO and pull down on SWCLK unless the device already include them internally. see below. Should I add them or not to my board with LPC54S018M?

ULINK2 User's Guide: Target Connectors 

pastedImage_4.png

pastedImage_2.png

pastedImage_3.png

 

Labels (1)
0 Kudos
Reply
1 Solution
3,507 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Bob,

Both of the SWDIO and SWDCLK signals have on-chip pull-up resistors as the following Fig from UM11155.pdf, so I think it is okay not to use any any external resistors.

But I have checked the schematics of LPC540xx, the SWDIO pin is connected with a 100K ohm resistor, so I think you can connect a 100K ohm resistor or not for the SWDIO pin, for the SWDCLK, it is unnecessary to connect any resistor.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

View solution in original post

0 Kudos
Reply
2 Replies
3,508 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Bob,

Both of the SWDIO and SWDCLK signals have on-chip pull-up resistors as the following Fig from UM11155.pdf, so I think it is okay not to use any any external resistors.

But I have checked the schematics of LPC540xx, the SWDIO pin is connected with a 100K ohm resistor, so I think you can connect a 100K ohm resistor or not for the SWDIO pin, for the SWDCLK, it is unnecessary to connect any resistor.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 Kudos
Reply
3,507 Views
belmontbob59
Contributor IV

thank you

0 Kudos
Reply