LPC54S018M: SWD's SWDIO and SWCLK pins pullup/pulldown

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC54S018M: SWD's SWDIO and SWCLK pins pullup/pulldown

跳至解决方案
3,672 次查看
belmontbob59
Contributor IV

KEIL recommends to add pull up on SWDIO and pull down on SWCLK unless the device already include them internally. see below. Should I add them or not to my board with LPC54S018M?

ULINK2 User's Guide: Target Connectors 

pastedImage_4.png

pastedImage_2.png

pastedImage_3.png

 

标签 (1)
0 项奖励
回复
1 解答
3,579 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Bob,

Both of the SWDIO and SWDCLK signals have on-chip pull-up resistors as the following Fig from UM11155.pdf, so I think it is okay not to use any any external resistors.

But I have checked the schematics of LPC540xx, the SWDIO pin is connected with a 100K ohm resistor, so I think you can connect a 100K ohm resistor or not for the SWDIO pin, for the SWDCLK, it is unnecessary to connect any resistor.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,580 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Bob,

Both of the SWDIO and SWDCLK signals have on-chip pull-up resistors as the following Fig from UM11155.pdf, so I think it is okay not to use any any external resistors.

But I have checked the schematics of LPC540xx, the SWDIO pin is connected with a 100K ohm resistor, so I think you can connect a 100K ohm resistor or not for the SWDIO pin, for the SWDCLK, it is unnecessary to connect any resistor.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 项奖励
回复
3,579 次查看
belmontbob59
Contributor IV

thank you

0 项奖励
回复