LPC54S018M: SWD's SWDIO and SWCLK pins pullup/pulldown

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54S018M: SWD's SWDIO and SWCLK pins pullup/pulldown

ソリューションへジャンプ
3,656件の閲覧回数
belmontbob59
Contributor IV

KEIL recommends to add pull up on SWDIO and pull down on SWCLK unless the device already include them internally. see below. Should I add them or not to my board with LPC54S018M?

ULINK2 User's Guide: Target Connectors 

pastedImage_4.png

pastedImage_2.png

pastedImage_3.png

 

ラベル(1)
0 件の賞賛
返信
1 解決策
3,563件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Bob,

Both of the SWDIO and SWDCLK signals have on-chip pull-up resistors as the following Fig from UM11155.pdf, so I think it is okay not to use any any external resistors.

But I have checked the schematics of LPC540xx, the SWDIO pin is connected with a 100K ohm resistor, so I think you can connect a 100K ohm resistor or not for the SWDIO pin, for the SWDCLK, it is unnecessary to connect any resistor.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,564件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Bob,

Both of the SWDIO and SWDCLK signals have on-chip pull-up resistors as the following Fig from UM11155.pdf, so I think it is okay not to use any any external resistors.

But I have checked the schematics of LPC540xx, the SWDIO pin is connected with a 100K ohm resistor, so I think you can connect a 100K ohm resistor or not for the SWDIO pin, for the SWDCLK, it is unnecessary to connect any resistor.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 件の賞賛
返信
3,563件の閲覧回数
belmontbob59
Contributor IV

thank you

0 件の賞賛
返信