LPC546xx mismatch between SDK and UM10912 static and dynamic memory region

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC546xx mismatch between SDK and UM10912 static and dynamic memory region

1,580 Views
danielgull
Contributor IV

Hi NXP community

I am using LPC546xx and have found a mismatch between the SDK 2.5.0 and User Manual UM10912 concerning static and dynamic memory regions depending on Cip Select:

Static Memory Chip Select Base address

CS0: 0x8000'000 (UM10912) vs 0x8000'0000 (SDK)

CS1: 0x8800'000 (UM10912) vs 0x9000'0000 (SDK)

CS2: 0x9000'000 (UM10912) vs 0x9800'0000 (SDK)

CS3: 0x9800'000 (UM10912) vs 0x9C00'0000 (SDK)

Dynamic Memory Chip Select Base address

CS0: 0xA000'000 (UM10912) vs 0xA000'0000 (SDK)

CS1: 0xA800'000 (UM10912) vs 0xB000'0000 (SDK)

CS2: 0xB000'000 (UM10912) vs 0xC000'0000 (SDK)

CS3: 0xB800'000 (UM10912) vs 0xD000'0000 (SDK)

Which one is the correct one? SDK or User Manual?

Dani

Labels (2)
4 Replies

1,394 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Daniel,

The UM10912 description is correct.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 Kudos
Reply

1,394 Views
danielgull
Contributor IV

Hi Rong

So how can I fit up to 256 MB into the dynamic memory sections without writing into the next section?

0xA000'0000 - 0xA7FF'FFFF allows a maximum of 128 MB NOT 256 MB.

I believe the User Manual is also wrong!

Dani

0 Kudos
Reply

1,394 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Daniel,

For the SDRAM address map Table, I think the size 256MB is correct, but the address range is incorrect.

Pls download the an12026.pdf from the link:

https://www.nxp.com/docs/en/nxp/application-notes/AN12026.pdf 

it gives the chip select for both DRAM and SRAM.

pastedImage_2.png

BR

XiangJun Rong

1,394 Views
danielgull
Contributor IV

Great information - thank you Rong - Wish you a great weekend. I should be able to work with this now.

Many thanks

Dani

0 Kudos
Reply