LPC546xx external NAND flash support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC546xx external NAND flash support

2,719件の閲覧回数
isaotakashima
Contributor IV

We have plan to make our new product using LPC546xx.

We want to use external parallel NAND flash to store a lot of sensor data about 128 MB - 1 GB.

According to below discussion, EMC supported LPC can support external parallel NAND flash.

https://community.nxp.com/message/762682 

Can LPC546xx also support external parallel NAND flash?

Please reply as soon as possible.

Best regards,

Takashima

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,589件の閲覧回数
isaotakashima
Contributor IV

According to the following discussion, LPC4367 can support external parallel NAND flash.

NAND Flash interface support in LPC4367 

Why EMC of LPC546xx cannot support external parallel NAND flash?


Please reply as soon as possible.

Best regards,

Takashima

0 件の賞賛
返信

2,589件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Isao,

I do not think that the EMC of LPC54xxx supports nand flash, the EMC supports only SDRAM,SRAM,parallel Nor flash,I suggest you use i.mxrt family for example i.mxrt1020/1050, which has SEMC module,can interface with NOR flash, SRAM,SDRAM,Nand flash.

i.MX RT Series: MCU/Applications Crossover Processor | Arm® Cortex®-M7 | NXP 

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信