LPC546xx external NAND flash support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC546xx external NAND flash support

2,638 Views
isaotakashima
Contributor IV

We have plan to make our new product using LPC546xx.

We want to use external parallel NAND flash to store a lot of sensor data about 128 MB - 1 GB.

According to below discussion, EMC supported LPC can support external parallel NAND flash.

https://community.nxp.com/message/762682 

Can LPC546xx also support external parallel NAND flash?

Please reply as soon as possible.

Best regards,

Takashima

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

2,508 Views
isaotakashima
Contributor IV

According to the following discussion, LPC4367 can support external parallel NAND flash.

NAND Flash interface support in LPC4367 

Why EMC of LPC546xx cannot support external parallel NAND flash?


Please reply as soon as possible.

Best regards,

Takashima

0 Kudos
Reply

2,508 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Isao,

I do not think that the EMC of LPC54xxx supports nand flash, the EMC supports only SDRAM,SRAM,parallel Nor flash,I suggest you use i.mxrt family for example i.mxrt1020/1050, which has SEMC module,can interface with NOR flash, SRAM,SDRAM,Nand flash.

i.MX RT Series: MCU/Applications Crossover Processor | Arm® Cortex®-M7 | NXP 

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply