LPC546xx and crystal-less USB0 operation in device mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC546xx and crystal-less USB0 operation in device mode

1,009件の閲覧回数
giusloq
Contributor III

It seems it's possible to use USB0 full-speed peripheral in device mode with only internal oscillator (without an external crystal).

However Errata says there's a problem with clock adjustment when the device is connected to the host through multiple bus. The work-around is:

Use the FRO calibration library provided in TN00032. This library allows the application to
have a crystal-less USB device operation in full-speed mode.

I tried to search for Technical Note TN00032, but I couldn't. Where is it?

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 返信

1,005件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You can download it from the link:

https://www.nxp.com/docs/en/application-note/TN00032.zip

If you can not download it, pls update the ticket, I will attach it here.

BR

XiangJun Rong

 

0 件の賞賛
返信