LPC546xx: USB interrupt pipe polling notification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC546xx: USB interrupt pipe polling notification

跳至解决方案
2,420 次查看
rex_lam
Contributor IV

Is there a way to be notified when the host polls the USB interrupt IN pipe? I looked at the USB example projects and it seems that USB0_IRQHandler is not triggered when the device has nothing to report, i.e. responds to the interrupt poll with NAK. I would like my code to be notified when it receives the interrupt IN poll from the host.

标签 (2)
1 解答
2,209 次查看
carstengroen
Senior Contributor II

Rex,

have a look at my post here: Custom USB class using USBROM (for LPC54608 and alike), code to grab  

(at the end of the page)

Basically I use

// Allow both acknowledged and NAK'ed  packets to generate interrupts (otherwise it is only acknowledged packets that generate interrupts)
LPC_USB0->DEVCMDSTAT |= (1<<12) | (1<<13);‍‍

在原帖中查看解决方案

2 回复数
2,210 次查看
carstengroen
Senior Contributor II

Rex,

have a look at my post here: Custom USB class using USBROM (for LPC54608 and alike), code to grab  

(at the end of the page)

Basically I use

// Allow both acknowledged and NAK'ed  packets to generate interrupts (otherwise it is only acknowledged packets that generate interrupts)
LPC_USB0->DEVCMDSTAT |= (1<<12) | (1<<13);‍‍
2,209 次查看
rex_lam
Contributor IV

Thank you Carsten.