LPC54618 External clock input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54618 External clock input

1,297件の閲覧回数
tijmen
Contributor I

Hello,

I want to drive the LPC54618 XTALIN input with a logic signal (3v3, 10 MHz) coming from a distributed clock signal. Is this possible and what hardware considerations should I take into account to make this possible?

Thanks for your reply.

Regards,

Tijmen van Eijk

ラベル(1)
0 件の賞賛
返信
1 返信

1,220件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Tijmen van Eijk,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
For the LPC546xx series, the oscillator input pin (XTALIN) cannot be driven by an external clock. Must connect a crystal between XTALIN and XTALOUT. In another word, it's unavailable to drive the LPC54618 via extern oscillator connect the XTALIN input pin.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信