LPC54618 External clock input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54618 External clock input

1,339 Views
tijmen
Contributor I

Hello,

I want to drive the LPC54618 XTALIN input with a logic signal (3v3, 10 MHz) coming from a distributed clock signal. Is this possible and what hardware considerations should I take into account to make this possible?

Thanks for your reply.

Regards,

Tijmen van Eijk

Labels (1)
0 Kudos
Reply
1 Reply

1,262 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Tijmen van Eijk,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
For the LPC546xx series, the oscillator input pin (XTALIN) cannot be driven by an external clock. Must connect a crystal between XTALIN and XTALOUT. In another word, it's unavailable to drive the LPC54618 via extern oscillator connect the XTALIN input pin.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply