LPC54616 SCTimer input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54616 SCTimer input

ソリューションへジャンプ
2,995件の閲覧回数
wangyanjun
Contributor II

As described in the manual, Tx_OUT0 can be used as SCTimer input.

But what is the Tx_OUT0? Is CTimer's match output or others?

0 件の賞賛
返信
1 解決策
2,973件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanJun,

Thank you for the feedback. If the CTimer is used to counts external clock, and you want to test the external signal clock frequency, you can use the CTimer as a divider, the CTimer outputting clock signal can function as a capture signal for the SCT, with the capture function, the SCT can test the external signal frequency.

BR

XiangJun Rong

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,985件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanJun,

As the following Fig shows, the Tx_OUT0 can be an input signal for the SCT module, the signal can function as capture signal, which can generate event with programmable rising/falling edges, if you enable an interrupt, the event can trigger an interrupt. With the capture function, user can test the width of the signal..

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1610435435898.png

 

0 件の賞賛
返信
2,980件の閲覧回数
wangyanjun
Contributor II

Thank you for your reply.

I found the answer from MCUxpresso Config Tools. The Tx_OUT0 is the CTimer's match channel 0 output.

0 件の賞賛
返信
2,974件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanJun,

Thank you for the feedback. If the CTimer is used to counts external clock, and you want to test the external signal clock frequency, you can use the CTimer as a divider, the CTimer outputting clock signal can function as a capture signal for the SCT, with the capture function, the SCT can test the external signal frequency.

BR

XiangJun Rong

 

0 件の賞賛
返信