LPC54616 SCTimer input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54616 SCTimer input

Jump to solution
2,993 Views
wangyanjun
Contributor II

As described in the manual, Tx_OUT0 can be used as SCTimer input.

But what is the Tx_OUT0? Is CTimer's match output or others?

0 Kudos
Reply
1 Solution
2,971 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanJun,

Thank you for the feedback. If the CTimer is used to counts external clock, and you want to test the external signal clock frequency, you can use the CTimer as a divider, the CTimer outputting clock signal can function as a capture signal for the SCT, with the capture function, the SCT can test the external signal frequency.

BR

XiangJun Rong

 

View solution in original post

0 Kudos
Reply
3 Replies
2,983 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanJun,

As the following Fig shows, the Tx_OUT0 can be an input signal for the SCT module, the signal can function as capture signal, which can generate event with programmable rising/falling edges, if you enable an interrupt, the event can trigger an interrupt. With the capture function, user can test the width of the signal..

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1610435435898.png

 

0 Kudos
Reply
2,978 Views
wangyanjun
Contributor II

Thank you for your reply.

I found the answer from MCUxpresso Config Tools. The Tx_OUT0 is the CTimer's match channel 0 output.

0 Kudos
Reply
2,972 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanJun,

Thank you for the feedback. If the CTimer is used to counts external clock, and you want to test the external signal clock frequency, you can use the CTimer as a divider, the CTimer outputting clock signal can function as a capture signal for the SCT, with the capture function, the SCT can test the external signal frequency.

BR

XiangJun Rong

 

0 Kudos
Reply